Skip to main content
Acane.11
Associate
May 11, 2020
Question

problem add service on gatt error 0x47, BlueNRG-2

  • May 11, 2020
  • 1 reply
  • 791 views

hi, i'm using steval-idb00bv2 board ans i want to add my custom service to the other present on the example that already read the sensor present on the board.

this is the code that i have added and give me the problem

#define COPY_RAICAM_DEMO_SERVICE_UUID(uuid_struct)  COPY_UUID_128(uuid_struct,0x00,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0x9a,0xb4,0x00,0x02,0xa5,0xd5,0xc5,0x1b)

#define COPY_BODY_TEMP_CHAR_UUID(uuid_struct) COPY_UUID_128(uuid_struct,0x00,0x00,0x00,0x00,0x00,0x01,0x11,0xe1,0xac,0x36,0x00,0x02,0xa5,0xd5,0xc5,0x1d)

tBleStatus Add_HWServW2ST_Service(void)

{

 tBleStatus ret;

uint8_t uuid1[16];

COPY_RAICAM_DEMO_SERVICE_UUID(uuid1);  

 Osal_MemCpy(&service_raicam_uuid.Service_UUID_128, uuid1, 16);

//https://community.st.com/s/question/0D50X00009XkYAvSAN/sensortile-bluenrgms-custom-service-aci

printf("provo ad aggiungere servizi\n") ;

 ret = aci_gatt_add_service(UUID_TYPE_128, &service_raicam_uuid, PRIMARY_SERVICE, 1+6, &RaicamDemoHandle); 

 if (ret != BLE_STATUS_SUCCESS) 

  { printf("errore 3\n") ;

return BLE_STATUS_ERROR;   

}

  

 /* Fill the Environmental BLE Characteristc */

 COPY_BODY_TEMP_CHAR_UUID(uuid);

 Osal_MemCpy(&char_uuid.Char_UUID_128, uuid, 16);  

// 2 byte timer + 2 byte temperatura + 4 byte pressione

 ret = aci_gatt_add_char(RaicamDemoHandle, UUID_TYPE_128, &char_uuid, 2+2, 

              CHAR_PROP_NOTIFY|CHAR_PROP_READ, 

              ATTR_PERMISSION_NONE, 

              GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,

              16, 0, &BodyTempCharHandle);

 if (ret != BLE_STATUS_SUCCESS) 

  { printf("error 4\n") ;

return BLE_STATUS_ERROR;   

}

 return BLE_STATUS_SUCCESS;

}

here the log from the uart

 0693W000000XCU9QAO.jpg

thanks for the support

    This topic has been closed for replies.

    1 reply

    Acane.11
    Acane.11Author
    Associate
    May 12, 2020

    Hi, at the end i found the solution myself by reading the document PM0257, here i report the extract. before use a service or attribute it is necessary to allocate the relative memory space as describe on the table with the function BlueNRG_Stack_Initialization(&BlueNRG_Stack_Init_params);.

    0693W000000XGkzQAG.jpg

    0693W000000XGlJQAW.jpg

    regards