Problem wih the SWD frequency speed in order to flash a BlueNRJ-232 chip.
Hello all,
I am using in my project a BlueNRG-232 chip in order to have a bluetooth function. I would like to speed UP the flash frequency of my BlueNRG chip. Currently I am limited to 50kHz and it is impossible to go up.
I am using a st link programmer V2 with the flasing software BlueNRJ-1 ST LINK utility.
I have checked all the wires, and they are ok. In addition, with the same connection, I can easily program the stm32 which drives the BlueNRG
Is it a frequent problem ? Has anyone ever encountered this issue ?
Best regards,