Question about the BlueNRG-2N Simultaneous Connections
Hi,
I was reading the BlueNRG-2N features on this datasheet, and it stated that it could "handle up to 8 simultaneous connections."
Does this mean that one GAP Central device based on the BlueNRG-2N could transmit up to 8 GAP Peripheral devices (also containing the BlueNRG-2N) at the exact same timeframe?
In the example above, if I were to transmit the same packet to 8 devices at t1 = x seconds, and if I set a connection length of ConnectionLength = y seconds for all the peripheral devices connected to it, all 8 peripherals would receive the packet at x + y + <some_hardware_overhead> seconds after it was transmitted by the GAP central device? Also, if all the GAP Peripheral devices were to send a message back through an Indicate/Notify operation, the GAP central could also receive all the Indicate/Notify messages from the 8 Peripheral devices at the same time?
Any clarification would be helpful. Thanks!