Snaphat M4T32-BR12SH6 - expected battery life is lower than 10 years
I'm using the snaphat M4T32-BR12SH6 (battery + crystal) with RTC M41T94.
The battery life is short, after less than 1 year, the battery voltage is lower than 2.5 V and the RTC does not work well.
And according to the datasheet, the minimum expected life is 10 years!
I suspect that the manufacturing date is old, probably manufactured in 2013, but could it still operate for another 3 years or not?