ST67W61 and H563ZI Nucleo
H563ZI Nucleo and Nucleo-67W61.
Using the CLI Binary version 1.1.0 I get:
#### Welcome to ST67W6X CLI Application #####
# build: 20:14:53 Sep 25 2025
--------------- Host info ---------------
Host FW Version: 1.1.0
[ERROR] [575] [spi_xfer_engine] (spi_iface.c:297) Invalid magic 0x5501
[ERROR] [575] [spi_xfer_engine] (spi_iface.c:512) Invalid spi header from peer, magic 0x5501, len (0, 0x0), version 0, type 0flags 0x0, rsvd 0x1
[ERROR] [2575] [spi_xfer_engine] (spi_iface.c:448) waiting for spi txn ready timeouted
[ERROR] [4000] [ST67W6XTask] (w61_at_common.c:375) sem_if_ready not received
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:314) Could not init Modem handler
[ERROR] [4000] [ST67W6XTask] (main_app.c:783) [ERROR] in W6X_Init API
[ERROR] [4000] [ST67W6XTask] (w6x_sys.c:101) W61 Init failed
[ERROR] [4000] [ST67W6XTask] (main_app.c:283) failed to initialize ST67W6X Driver, 2
##### Application end
Suggestions? Thank you.