ST67W61M1 Connection Errors and DTIM Issue
Hi,
I am currently working on a feasibility project using the X-NUCLEO-67W61M1 and NUCLEO-U575ZI-Q.
The sample code I am using is ST67W6X_FOTA.
The FOTA functionality is working properly. However, during the initial connection phase, there is about a 50% chance of encountering Wi-Fi connection-related errors. The errors I have observed include:
"Wi-Fi connect timeouted"
"Wi-Fi connect in error"
"Failed to initialize the DTIM"
Whenever these issues occur, the only way to recover is by resetting the MCU and restarting the process.
Are there any recommended methods or best practices to resolve these issues?