Skip to main content
Visitor II
January 10, 2024
Question

STEVAL-FKI433V2 send custom data on GPIO

  • January 10, 2024
  • 0 replies
  • 512 views

Hi, I'm new with this development board.

My target is to use the S2-LP DK Application to configure the board to send data from a GPIO.

Do I have to put my data on GPIO_0 and the clock signal to GPIO_1?

Why is the clock signal needed?

In this way it is possible to change also the modulation? For example I want to send my packet on OOK mode or FSK mode.

 

Thanks

This topic has been closed for replies.