Skip to main content
RRich.3
Visitor II
May 10, 2021
Question

STEVAL-IDB005V1 and STEVAL-IDB006V1 problems

  • May 10, 2021
  • 1 reply
  • 578 views

I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10 so I can't use the GUI to update the Bluetooth stack. Any help would be appreciated.

I also have an STEVAL-IDB006V1 that does enumerate but does not advertise. Any help would be appreciated.

Thanks

    This topic has been closed for replies.

    1 reply

    Winfred LU
    ST Employee
    May 11, 2021

    >I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10

    It the board powered on? Check the power option.

    Do you see anything from the Device Manager? Try to flash the onboard STM32L from the JTAG connector, with the prebuilt VCOM firmware image in DK.

    >I also have an STEVAL-IDB006V1 that does enumerate but does not advertise

    I guess you need to configure it to advertise accordingly. Can you connect it with the GUI?