STM32L072 - VDD_USB Supply Current (for PA11, PA12)
PA11 and PA12 are powered from VDD_USB.
So, to use PA11 and/or PA12, we have to have the VDD_USB domain powered-up.
I can't find any documentation of the expected VDD_USB current draw when the USB functionality is not used.
In a previous project, I remember noticing that it did cause some extra current drain - but I don't recall how much.
So the question is: what is the expected VDD_USB current draw when the USB functionality is not used?
(this is with specific reference to the B-L072Z-LRWAN1 board - where PA12 is used to power the TCXO)