STUSB4710: Default Configuration Confirmation
Hello,
I apologize if the answer is obvious but I want to confirm my understanding for the STUSB4710 (USB-C PD controller). Section 4.1 of the datasheet mentions that the default values for the voltage and current settings, which require NO I2C programming. I can optionally choose to overwrite these values via an I2C interface if I want.
So if I use the 7.1. configuration, this means that, with no additional MCU, EEPROM or any other NVM, I can achieve:
5V, 3A (15W)
9V, 3A (27W)
12V, 3A (36W)
15V, 3A (40W)
20V, 2.25A (45W)
Is this logic correct?