SWD connection to BlueNRG-LP failed - IDB011V1 CMSIS-DAP, RF Flasher Utility
I'm working with (still) IDB011V1. There is an issue with using SWD connection to BlueNRG-LP. I can connect to the device via SWD, when the device is erased via UART, but after I flash the BlueNRG-LP, I can't connect it via SWD anymore.
Any solution for it?
******MASS ERASE OPERATION******
Mass Erase Boards: COM8 (ST DK)
10:01:56.838: Device COM8 (ST DK) -> Mass Erase: Started
10:01:58.548: Device COM8 (ST DK) -> Mass Erase: Finished
10:01:58.548: Device COM8 (ST DK) -> Mass Erase: Flash memory successfully erased.
******START FLASH OPERATION******
Flash Boards: COM8 (ST DK)
10:02:33.064: Device COM8 (ST DK) -> Device Identification
10:02:34.406: Device COM8 (ST DK) -> Flash Programming...
10:02:36.414: Device COM8 (ST DK) -> Flash Programming: SUCCESS.
10:02:36.438: Device COM8 (ST DK) -> Flash Memory Verifying...
10:02:39.422: Device COM8 (ST DK) -> Flash Memory Verifying: SUCCESS.
******END FLASH OPERATION******
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:02:47.741: Waiting device to read (device connected by CMSIS-DAP) ->FAILED. (It's not possible to connect to the device)
******MASS ERASE OPERATION******
Mass Erase Boards: COM8 (ST DK)
10:03:00.834: Device COM8 (ST DK) -> Mass Erase: Started
10:03:02.531: Device COM8 (ST DK) -> Mass Erase: Finished
10:03:02.531: Device COM8 (ST DK) -> Mass Erase: Flash memory successfully erased.
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:08.133: Waiting device to read (device connected by CMSIS-DAP) ->Device Connected
10:03:09.345: Device Identification -> BlueNRG-LP
10:03:10.444: Read Flash Memory -> SUCCESS
10:03:12.528: Device Disconnection -> SUCCESS
******FLASH OPERATION******
Flash of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:27.531: Device connection by CMSIS-DAP -> Device connected
10:03:28.641: Device Identification -> BlueNRG-LP
10:03:29.707: Device Flash Programming -> SUCCESS (Flash Programmed in 2.763541 sec.)
10:03:32.471: Flash Verify Operation -> SUCCESS
10:03:33.783: Device Disconnection -> SUCCESS
10:03:35.484: Flash operation finished!
******END FLASH OPERATION******
******FLASH READ OPERATION******
Read of n.1 device connected by SWD (ST-Link/V2, CMSIS-DAP, J-Link)
10:03:39.981: Waiting device to read (device connected by CMSIS-DAP) ->FAILED. (It's not possible to connect to the device)