The aci_gap_pairing_complete_event is not called for random passkey response on version V1.0.0 ?
Which stack release do I need to pull this in, I am currently using V1.0.0.
The issue I see, seems similar, where in I don't see the paring complete ever being called (rarely called or not returned at all).
My Initiator parameters are (BLE112D)
Io capability 7 (Display with Keyboard), mitm enabled, encryption key min size 7, bonding enabled.
The peripheral is a bluenrg, with authentication details.
ret = aci_gap_set_authentication_requirement( BONDING,
MITM_PROTECTION_REQUIRED,
SC_IS_SUPPORTED,
KEYPRESS_IS_NOT_SUPPORTED,
7,
16,
DONOT_USE_FIXED_PIN_FOR_PAIRING,
pincode,
PUBLIC_ADDR);
Are these requirements for authentication valid ?
And does this seem a relatable issue to ID 5284?