Skip to main content
JMüll.1
Associate II
October 3, 2020
Solved

Unable to get the provided sample apps (Sensorapp and sampleapp) running on a Nucleo-STM32F411RE with a X-Nucleo-BNRG2A1 expansion.

  • October 3, 2020
  • 1 reply
  • 828 views

I try to get the sample app and the sensor app running on a Nucleo-STM32F411RE together with a X-Nucleo-BNRG2A1 expansion. I configured everything as it was described in the corresponding docu. But I was not able to get it running. The device does not even show up in a Bluetooth scanner. I setup the same board with the older X-Nucleo-IDB05A1 many times and had no problems getting it running. Is there anything that is different with the X-Nucleo-BNRG2A1 expansion? I alread checked the jumpers. J10 is connected. J14 connects Pins 2 and 3. and J15 is open. What am i doing wrong here? I tried to debug the applications and found out that the hci_*** command don't return the BLE_STATUS_SUCCESS as they should do.

Thank you very much for your help.

This topic has been closed for replies.
Best answer by JMüll.1

Problem is solved! I used the existing video for setting up the STM32F411RE board together with the BNRG2A1 expansion. There are some important differences to the old expansion board which didn't recognized at the beginning.

1 reply

JMüll.1
JMüll.1AuthorBest answer
Associate II
October 4, 2020

Problem is solved! I used the existing video for setting up the STM32F411RE board together with the BNRG2A1 expansion. There are some important differences to the old expansion board which didn't recognized at the beginning.