Skip to main content
Breukers.Ron
Associate II
June 20, 2022
Question

Update rate LIV3F

  • June 20, 2022
  • 2 replies
  • 984 views

We are using the LIV3F in our project. We need an effective output data rate of at least 2 updates per second.

I set the update rate at 4 updates/second ($PSTMSETPAR,1303,0.25,0*1F\n\r").

I selected only GPRMC and GPGGA messages. me($PSTMCFGMSGL,0,1,00000042,00000000*4A\r\n",39).

Without GPS lock it does output at 4 updates/second. However as soon as GPS is locked, the data rate becomes very variable and has an average of 1.5 updates/second.

Itried switching off the low power mode ($PSTMCFGLPA,0,1,10,2,8,60,180,0,0,15,9,100,0*20\r\n",49) without difference.

Of course I save the parameters ($PSTMSAVEPAR*58\r\n",17)

All other parameters are default. Software version 4.6.8.2

What do I do wrong?

    This topic has been closed for replies.

    2 replies

    Breukers.Ron
    Associate II
    June 20, 2022

    A short additional observation. It happens that there is a gap of sometimes many seconds between data transfers. I check with an oscilloscope and at the same time I am logging the data. After such a gap, all the records which are missed come bunched together all at the same time. See the attached data record.

    Breukers.Ron
    Associate II
    June 21, 2022

    I found the solution. You need to increase the clock of the LIV3F CPU using the command "$PSTMSETPAR,1130,00,0*04\r\n"

    It is mentioned in the software manual but ONLY in footnote!!!