What is the maximum SPI speed and MCU system clock which can be configured for using BlueNRG2-M2SP module with it
Hello,
in the X-CUBE-BLE package this document STMicroelectronics.X-CUBE-BLE2_GettingStarted.pdf says the maximum SPI frequency could be 1Mbits/s .
In high perf MCU running at SysClock >500 Mhz , is it possibe to interface BlueNRG2 with it?
using Clock generator we are able to achieve the SPI speed < 1000 Kbits/s but i want to know the considerations which we need to take care as we are seeing some intermittent ble disconnection and some times no advertising.
Regards,
Darla