Why S2LP does not work at low temperatures?
I use S2LP at 433 MHz with proprietary narrowband protocol. Crystal 25 MHz 10 ppm XRCGB25M000F1H02R0 from Murata; capacitors 18 pF.
Devices operate OK if ambient temperature is positive. When I put them into freezer they stop responding to the base station. Devices are temperature dataloggers. While being in freezer, they continue to log temperatures, and we can see that microcontroller works OK down to -17 C. But S2LP stops responding at temperatures around 0 C.
I suspect that S2LP oscillator does not start if it is cold. Did anyone experienced similar problems?