X-NUCLEO-67W61M1 + NUCLEO-F446RE compatibility — HardFault in FreeRTOS xQueue (ST67W6X_CLI)
- November 3, 2025
- 3 replies
- 419 views
Dear ST Support Team,
I’m currently trying to run the ST67W6X_CLI application (from the Wi-Fi ST67W6X CLI Wiki)
using the following setup:
Wi-Fi Expansion Board: X-NUCLEO-67W61M1
Host MCU Board: NUCLEO-F446RE
IDE: STM32CubeIDE (latest version)
Middleware: FreeRTOS (as provided in the ST67W6X_CLI example)
The project builds successfully and the firmware is programmed without errors, but at runtime, I encounter a HardFault_Handler.
The fault occurs inside the FreeRTOS queue management code, specifically during a call to xQueueReceive() in queue.c.
Debug Information:
When the fault occurs, the debugger stops inside:
prvCopyDataFromQueue(pxQueue, pvBuffer);
and the corrupted member is:
pxQueue->uxItemSize
Observed value: 536871212 (0x2000412C) — which clearly points to an invalid or corrupted queue structure.
Call stack snapshot:
HardFault_Handler()
prvCopyDataFromQueue() at queue.c
xQueueReceive() at queue.c
spi_get_txbuf() at spi_iface.c
Please see the attached screenshot (from STM32CubeIDE) showing the variable states at the moment of the fault.
Runtime Log Output (During Debugging Only):
#### Welcome to ST67W6X CLI Application #####
build: 02:35:06 Nov 3 2025
--------------- Host info ---------------
Host FW Version: 1.1.0
[ERROR] [4000] [ST67W6XTask] (w61_at_common.c:375) sem_if_ready not received
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:314) Could not init Modem handler
[ERROR] [4000] [ST67W6XTask] (main_app.c:791) [ERROR] in W6X_Init API
[ERROR] [4000] [ST67W6XTask] (w6x_sys.c:101) W61 Init failed
[ERROR] [4000] [ST67W6XTask] (main_app.c:291) failed to initialize ST67W6X Driver, 2
Application end
Note:
This output appears only during debugging. When the application is executed standalone (without debugger), no console output appears and initialization fails silently.
What I Have Verified So Far:
The project compiles and links successfully without any warnings or missing paths.
I have configured FreeRTOS parameters exactly as recommended in the CLI_App Example (including heap size and default task stack).
The configTOTAL_HEAP_SIZE and task stack sizes match the reference configuration.
some custom modifications were made to (fota.c).
The same application is confirmed to work on NUCLEO-U575ZI-Q, NUCLEO-H563ZI, and other officially supported boards.
Important Note on Module Firmware:
So far, I have only flashed the host MCU (NUCLEO-F446RE) with the CLI example firmware.
I did not flash any binary to the ST67W6X module itself.
Could the issue (sem_if_ready not received and W61 Init failed) be caused by missing or outdated firmware on the Wi-Fi module?
Questions:
Could this HardFault be due to memory alignment, DMA transfer, or structure packing differences on STM32F4 compared to the U5/H5 families?
Are there any additional adjustments to FreeRTOS memory or SPI interface required to make this demo compatible with F4 series MCUs?
- Should the ST67W6X module firmware also be updated or flashed before running the CLI application?
- If yes, could you please confirm if this file NCP_update_mission_profile_t01.bat in the path: x-cube-st67w61\Projects\ST67W6X_Utilities\Binaries is the required one or not?