Skip to main content
Javi
Visitor II
July 30, 2020
Question

X-NUCLEO-IDW0M1 examples doesn't work for Nucleo-F401RE (HAL_UARTx_Receive_IT Error)

  • July 30, 2020
  • 0 replies
  • 482 views

Hello,

I'm trying to run the examples for X-NUCLEO-IDW0M1 WiFi expansion board and they doesn't work.

I'm using a nucleo F401RE which is supposed to be compatible with this expansion board. I just plug both boards and run the examples. Once the program is running I used the default SSID configuration (which I modified to be my own router configuration) and then the program gets stuck initializing the wifi module. Like the following picture:

0693W000003BlQFQA0.jpg

After waiting for a while it prints HAL_UARTx_Receive_IT Error a lots of times.

0693W000003BlRmQAK.jpg

I use the debug tool and it get stuck in the wifi_init()--> wifi_reset() and hung in this loop:

while(IO_status_flag.WiFi_WIND_State.WiFiHWStarted != WIFI_TRUE)

{

__NOP(); //nothing to do

}

Can anyone help me please? It is the second board that I used for this project because I think that the other one was no compatible, but I have the same error and I don't know what to do.

Thank you.

    This topic has been closed for replies.