Skip to main content
Associate III
August 4, 2025
Question

About ASM330LHH STATUS_REG

  • August 4, 2025
  • 1 reply
  • 161 views

Please tell me about the STATUS_REG for ASM330LHH. I'm using SPI communication. A similar question was posted earlier, but the situation is slightly different.

When I ran the same program on 30 board-mounted samples, 29 of them showed a change in STATUS_REG within 400ms after the ASM330LHH setting, but one remained 0 without any change.

I'm guessing from this that is not a sowtware problem, but I would appriciate a list of possible factors as the cause.

1 reply

Federica Bossi
Technical Moderator
December 24, 2025

Hi @ggob ,

The STATUS_REG indicates new accelerometer and gyroscope data availability. If one board shows no change, possible causes include hardware issues (sensor damage, poor SPI connection, power problems), SPI communication errors (wrong settings, signal noise), incomplete sensor initialization, or the sensor being in low-power mode. I recommend checking SPI signals, power supply and comparing initialization across boards to isolate the issue.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.