AlgoBuilder FW for SensorTile.Box PRO does not stream any data
Hello, I am trying to build a simple firmware for my SensorTile.Box PRO to stream any data.
Using MEMS Studio's AlgoBuilder, I have set the correct Toolchain (STM32CubeIDE), and the target (SensorTile.box Pro). Then I built a simple design with Quaternions 9X attached to the Sensor Hub (Data Rate: Timer/100, Accelerometer Full Scale: 2g, Gyroscope Full Scale: 245dps), outputting to a Fusion component. I can generate C code and build and program my device in DFU mode.
However, when I connect it over Serial after rebooting the device, I can connect to it but the "play" button is grayed out and I cannot stream any data.
Using STM32CubeProgrammer to flash other compatible firmware that came with MEMS Studio (steval-mkboxpro, steval-mkboxpro-ble), I can connect and stream (play button is enabled) data as per normal so I doubt the problem lies with the hardware.
I have also tried other designs with SensorHub -> Any other sensors -> Value instead of Quaternions 9X, but none of it worked.
Any help is appreciated, thank you!