Skip to main content
Visitor II
September 26, 2024
Question

ASM330:Filter link and gyroscope transfer function of asm330 gyroscope.

  • September 26, 2024
  • 1 reply
  • 577 views

The filter link of asm330 gyroscope includes LPF1 and LPF2, in which LPF1 can be configured with bandwidth, and LP2 is related to ODR. May I ask how much phase shift is corresponding to each filter in different bandwidth or configuration mode? Or could you provide the transfer function of the gyroscope? I need to analyze the frequency characteristics of the gyroscope under different configurations to meet the requirements of the system I designed, thank you!

1 reply

Federica Bossi
Technical Moderator
November 8, 2024

Hi @BIAN ,

 

We can't share these data on st community. If you are interested in, you can open a ticket to the online support at this link.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.