Skip to main content
Associate III
September 2, 2025
Solved

ASM330LHH ODR and FS operating procedures.

  • September 2, 2025
  • 1 reply
  • 526 views

Can I operate ODR_XL[3:0], FS[1:0]_XL and LPF2_XL_EN of CTRL1_XL of ASM330LHH simultaneously?
Should I set FS[1:0]_XL and LPF2_XL_EN first and then set ODR_XL[3:0]?

Best answer by Federica Bossi

Hi @ggob ,

You can configure ODR_XL[3:0],FS[1:0]_XL, andLPF2_XL_ENbits of theCTRL1_XLregister in the ASM330LHH simultaneously in a single write operation, as they reside in the same register.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
September 11, 2025

Hi @ggob ,

You can configure ODR_XL[3:0],FS[1:0]_XL, andLPF2_XL_ENbits of theCTRL1_XLregister in the ASM330LHH simultaneously in a single write operation, as they reside in the same register.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.