Skip to main content
Associate
December 12, 2023
Question

BlueCoin入门套件

  • December 12, 2023
  • 2 replies
  • 967 views

BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊

 

This topic has been closed for replies.

2 replies

Federica Bossi
Technical Moderator
December 12, 2023

Hi @insist_66 ,

The BlueCoin can work at a maximum of 16kHz.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
insist_66Author
Associate
December 12, 2023

The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved

Federica Bossi
Technical Moderator
December 14, 2023

Hi @insist_66 ,

Unfortunately this is not possible: the library only works up to 16KHz, both input and output.
We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.