Skip to main content
Associate II
July 28, 2025
Question

Check configuration on lsm6dso32

  • July 28, 2025
  • 1 reply
  • 327 views

Hi! 

I inherited a project and we're seeing strange accelerometer values and I'd like to get a sanity check on my configuration. when Idle and flat, I see 1g on Z, 0g on X and Y. When my device is moving I see peaks on many axes beyond 1g, eg 2.5 on X or Z, and it does not seem real. Here is downsampled data from a log file. X (brown) goes from +1.5g to -1.5g, Z (gray) is over 2.3g. I am not expecting such numbers during a short banked turn at ~15 mph 

ms360_0-1753746022179.png

This is my init. I'm expecting 104Hz data rate, 4g acc scale, 1000dps gyrp scale

	m_dev_ctx.write_reg = (stmdev_write_ptr) STWriteRegister;
	m_dev_ctx.read_reg = (stmdev_read_ptr) STReadRegister;

	lsm6dso32_reset_set(&m_dev_ctx, PROPERTY_ENABLE);

	do
	{
		lsm6dso32_reset_get(&m_dev_ctx, &rst);
	}
	while (rst);

	/* Enable Block Data Update */
	lsm6dso32_block_data_update_set(&m_dev_ctx, PROPERTY_ENABLE);

	/* Set Output Data Rate */
	lsm6dso32_xl_data_rate_set(&m_dev_ctx, LSM6DSO32_XL_ODR_104Hz_HIGH_PERF);
	lsm6dso32_gy_data_rate_set(&m_dev_ctx, LSM6DSO32_GY_ODR_104Hz_HIGH_PERF);
	// lsm6dso32_fifo_data_rate_set(&m_dev_ctx, lsm6dso32_GY_ODR_104Hz);

	/* Set full scale */
	lsm6dso32_xl_full_scale_set(&m_dev_ctx, LSM6DSO32_4g);
	lsm6dso32_gy_full_scale_set(&m_dev_ctx, LSM6DSO32_1000dps);

	lsm6dso32_timestamp_set(&m_dev_ctx, 1);

	//set watermark level to 2 samples
	lsm6dso32_fifo_watermark_set(&m_dev_ctx, 2);

	lsm6dso32_pin_int1_route_t int1_set = {};
	int1_set.int1_ctrl.int1_fifo_th = 1;
	results = lsm6dso32_pin_int1_route_set(&m_dev_ctx, &int1_set);

	uint8_t value = 0x44;//accell and gyro
	int ret = lsm6dso32_write_reg(&m_dev_ctx, LSM6DSO32_FIFO_CTRL3, &value, 1);

	uint8_t value = 0x06;
	int ret = lsm6dso32_write_reg(&m_dev_ctx, LSM6DSO32_FIFO_CTRL4, &value, 1); //ne

... skipping motion FX init b/c the raw accel data looks bad. 

 Data acquisition after INT1 -> process in app scheduler. Apologies for sloppy indenting. I didn't fix it yet. 

lsm6dso32_fifo_tag_t reg_tag;
 /* Read number of samples in FIFO */
 lsm6dso32_fifo_data_level_get(&m_dev_ctx, &num);
 int i=0;
 int t=0;
 // NRF_LOG_ERROR("IMU SAMPLES: %d",num);
 while (num--) {
 
 /* Read FIFO tag */
 lsm6dso32_fifo_sensor_tag_get(&m_dev_ctx, &reg_tag);
 uint8_t buffer[6];
 
 switch (reg_tag) {
 case LSM6DSO32_XL_NC_TAG:
 memset(&m_imu_raw_sample_buffer[i].m_raw_imu_values[3], 0x00, 3 * sizeof(int16_t));
 lsm6dso32_fifo_out_raw_get(&m_dev_ctx, (uint8_t *)&m_imu_raw_sample_buffer[i].m_raw_imu_values[3]);
 i++;
 break;
 
 case LSM6DSO32_GYRO_NC_TAG:
 memset(&m_imu_raw_sample_buffer[t].m_raw_imu_values[0], 0x00, 3 * sizeof(int16_t));
 lsm6dso32_fifo_out_raw_get(&m_dev_ctx, (uint8_t *)&m_imu_raw_sample_buffer[t].m_raw_imu_values[0]);
 t++;
 break;
 
 default:
 /* Flush unused samples */
 }
 }
 for (int y=0;y<i; y++)
 {
 IMU_Process_Data(&m_imu_raw_sample_buffer[y].m_raw_imu_values[3], &m_imu_raw_sample_buffer[y].m_raw_imu_values[0]);
 }
 

 

1 reply

Federica Bossi
Technical Moderator
July 29, 2025

Hi @ms360 ,

We don't expect such values. Could you try repeating the test by implementing our examples available on GitHub? Just to exclude any issues related to your code.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ms360Author
Associate II
July 29, 2025

Thanks Federica. Bench testing always looks good. I get about 1G magnitude between the 3 axes. Even motion FX shows good rotation data on the bench. 

Field data is always where we see the weird values. Our logging is only at 4Hz due to space constrictions. 
I'll compare your github examples against what we have, and go from there. 

Is there any reason a sampling rate of 104 hz is risky? The examples have lower sample rates. 
Is there any documentation of sampling rate minimums to use with Motion FX? 

ms360Author
Associate II
July 30, 2025

@Federica Bossi I am noticing some small and large differences from your example code.
I'm going to add batch rates, stream mode, disable I3C and pull out sensor hub and the extra registers and do some field testing. 

 

The code I've inherited does not 

  • disable i3c
  • different sample rates (slower)
  • set batch rate 
  • set stream mode

The code I have inherited does

  • use LSM6DSOHub / sensor hub 
  • set extra registers
 uint8_t value = 0x44;//accell and gyro

 int ret = lsm6dso32_write_reg(&m_dev_ctx, LSM6DSO32_FIFO_CTRL3, &value, 1);

...
 uint8_t value = 0x06;

 int ret = lsm6dso32_write_reg(&m_dev_ctx, LSM6DSO32_FIFO_CTRL4, &value, 1); //ne