Skip to main content
Geoffrey Raynal
Visitor II
June 9, 2017
Question

data ready interrupt lsm6dsl

  • June 9, 2017
  • 1 reply
  • 956 views
Posted on June 09, 2017 at 16:37

Hello everyone,

I Would like read the lsm6dsl data by interrupt using the pin int1 on the sensor.

I configured the accelerometer ODR to 104 Hz

And i set up registers as follow :

 - Control_3C (0x12) =  64 (Data updated only when register has been readed / Interrupt level High / interrupt pin in push pull)

- Int1_CTRL (0x0d) = 1 (INT1_DRDY_XL enabled)

I get the first rising edge on int1 pin, this edge is detected by my MCU, I read status register and accelerometer datas but the int1 pin of the lsm6dsl stay in high level. How may I clear this interruption for the next set of data ?

Datasheet v : 

DocID028475 Rev 6

Thanks

Geoffrey

1 reply

ST Employee
June 12, 2017
Posted on June 12, 2017 at 10:37

The interrupt is reset when the higher part of one of the enabled channels is read (29h, 2Bh, 2Dh for the accelerometer).

Visitor II
April 9, 2025

Is this indicated in the datasheet ?