Skip to main content
Associate
November 18, 2023
Question

Enabling FIFO on LSM6DSOX

  • November 18, 2023
  • 11 replies
  • 5518 views

Hi, 

 

I'm trying to get the FIFO working on the LSM6DSOX on a custom board with a silicon labs microcontroller, communicating both through SPI.

 

I have checked the application note at https://www.st.com/resource/en/application_note/an5272-lsm6dsox-alwayson-3axis-accelerometer-and-3axis-gyroscope-stmicroelectronics.pdf and followed the example code at https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dsox_STdC/examples/lsm6dsox_fifo.c, but no success, so I'm wondering if I'm missing something or it's a hardware problem. 

 

I'm able to read the device id and communicate normaly with the IMU through SPI, retrieving acc and gyro readings without issues.

 

This is my code for enabling the FIFO:

 

 lsm6dsox_reset_set(&imu_dev, PROPERTY_ENABLE);
 uint8_t rst;
 do {
 lsm6dsox_reset_get(&imu_dev, &rst);
 } while (rst);

 /* Disable I3C interface */
 lsm6dsox_i3c_disable_set(&imu_dev, LSM6DSOX_I3C_DISABLE);
 /* Enable Block Data Update */
 lsm6dsox_block_data_update_set(&imu_dev, PROPERTY_ENABLE);
 /* Set full scale */
 lsm6dsox_xl_full_scale_set(&imu_dev, LSM6DSOX_2g);
 lsm6dsox_gy_full_scale_set(&imu_dev, LSM6DSOX_2000dps);
 /*
 * Set FIFO watermark (number of unread sensor data TAG + 6 bytes
 * stored in FIFO) to 10 samples
 */
 lsm6dsox_fifo_watermark_set(&imu_dev, 10);
 /* Set FIFO batch XL/Gyro ODR to 12.5Hz */
 lsm6dsox_fifo_xl_batch_set(&imu_dev, LSM6DSOX_XL_BATCHED_AT_12Hz5);
 lsm6dsox_fifo_gy_batch_set(&imu_dev, LSM6DSOX_GY_BATCHED_AT_12Hz5);
 /* Set FIFO mode to Stream mode (aka Continuous Mode) */
 lsm6dsox_fifo_mode_set(&imu_dev, LSM6DSOX_STREAM_MODE);
 /* Enable drdy 75 μs pulse: uncomment if interrupt must be pulsed */
 //lsm6dsox_data_ready_mode_set(&imu_dev, LSM6DSOX_DRDY_PULSED);
 /* Uncomment if interrupt generation on Free Fall INT1 pin */
// lsm6dsox_pin_int1_route_t int1_route;
// lsm6dsox_pin_int1_route_get(&imu_dev, &int1_route);
// int1_route.fifo_th = PROPERTY_ENABLE;
// int1_route.fifo_full = PROPERTY_ENABLE;
// int1_route.fifo_ovr = PROPERTY_ENABLE;
// int1_route.fifo_bdr = PROPERTY_ENABLE;
// lsm6dsox_pin_int1_route_set(&imu_dev, int1_route);
 /* Uncomment if interrupt generation on Free Fall INT2 pin */
// lsm6dsox_pin_int2_route_t int2_route;
// lsm6dsox_pin_int2_route_get(&imu_dev, NULL, &int2_route);
// int2_route.fifo_th = PROPERTY_ENABLE;
// int2_route.fifo_bdr = PROPERTY_ENABLE;
// int2_route.fifo_full = PROPERTY_ENABLE;
// int2_route.fifo_ovr = PROPERTY_ENABLE;
// lsm6dsox_pin_int2_route_set(&imu_dev, NULL, int2_route);
 /* Set Output Data Rate */
 lsm6dsox_xl_data_rate_set(&imu_dev, LSM6DSOX_XL_ODR_12Hz5);
 lsm6dsox_gy_data_rate_set(&imu_dev, LSM6DSOX_GY_ODR_12Hz5);

 

(the lines that are commented are not exactly the same on the sample, as they didn't match actual reg type declarations) and for reading the FIFO I have:

 

uint8_t imu_read_fifo(bool read_acc, bool read_gyro, uint8_t *buffer, uint8_t max_samples_read, uint8_t* samples_read){

 uint8_t wmflag = 0;

 lsm6dsox_fifo_wtm_flag_get(&imu_dev, &wmflag);

 while (!wmflag) {
 lsm6dsox_fifo_wtm_flag_get(&imu_dev, &wmflag);
 }
 *samples_read = 0;
 uint16_t fifo_num_samples;
 lsm6dsox_fifo_data_level_get(&imu_dev, &fifo_num_samples);
 *samples_read = 0;
 if (fifo_num_samples == 0){
 return SL_STATUS_OK;
 } else if (fifo_num_samples < max_samples_read){
 max_samples_read = fifo_num_samples;
 }

 uint8_t data_len = 0;
 while (*samples_read < max_samples_read){
 uint8_t* acc_data = &buffer[data_len];
 uint8_t* gyro_data = &buffer[data_len + read_acc ? 6 : 0];
 imu_read_fifo_measure_nc(read_acc, read_gyro, acc_data, gyro_data);
 data_len += read_acc ? 6 : 0;
 data_len += read_gyro ? 6 : 0;
 (*samples_read) ++;
 }
 //lsm6dsl_fifo_raw_data_get(&imu_dev, buffer, len);
}

void imu_read_fifo_measure_nc(bool read_acc, bool read_gyro, uint8_t *acc_data, uint8_t *gyro_data){
 uint8_t dummy_data[6];
 uint8_t sensor_tag;

 uint16_t fifo_num_samples;
 lsm6dsox_fifo_data_level_get(&imu_dev, &fifo_num_samples);

 while (fifo_num_samples && (read_acc || read_gyro)){
 lsm6dsox_fifo_sensor_tag_get(&imu_dev, &sensor_tag);
 switch (sensor_tag) {
 case LSM6DSOX_XL_NC_TAG:
 lsm6dsox_fifo_out_raw_get(&imu_dev, acc_data);
 read_acc = false;
 break;
 case LSM6DSOX_GYRO_NC_TAG:
 lsm6dsox_fifo_out_raw_get(&imu_dev, gyro_data);
 read_gyro = false;
 break;
 default:
 lsm6dsox_fifo_out_raw_get(&imu_dev, dummy_data);
 }
 fifo_num_samples --;
 }
}

 

But the watermark flag never changed and I get stuck in the while loop. I have tried also placing the execution on the reading part, but I didn't get anything when calling lsm6dsox_fifo_data_level_get.

 

If there is no a hardware problem, I think maybe I'm missing a trigger condition for the FIFO, or anything else is needed for enablling it.

 

I have searched elsewhere and I found references to use compression which require enabling something else, but I didn't found specific references to that being required for just using the FIFO (neither I would need the watermark or the interrupt, I just need to buffer some samples while I'm writing a previous batch on a flash memory which uses the same SPI line and can operate on a poll basis).

 

I also found something related to timestamping samples:

 

 lsm6dsox_fifo_timestamp_decimation_set(&imu_dev, LSM6DSOX_DEC_1);
 lsm6dsox_timestamp_set(&imu_dev, PROPERTY_ENABLE);
 lsm6dsox_fifo_timestamp_decimation_set(&imu_dev, LSM6DSOX_NO_DECIMATION);

 

Playing with this, I was able to trigger the watermark, and data_level_get returns non 0 content, but lsm6dsox_fifo_sensor_tag_get(&imu_dev, &sensor_tag) gives sensor_tag = 0x00 (by the way, the switch case on the lsm6dsox_fifo_sensor_tag_get function defaults to GYRO_NC_TAG, https://github.com/STMicroelectronics/lsm6dsox-pid/blob/3c2d02b69cb18de0cabd94c15dcd73aab6bd6edb/lsm6dsox_reg.c#L7584, what leads to misinterpret that a gyro reading is retrieved when the sensor_tag reports 0, which was my case). And lsm6dsox_fifo_out_raw_get also return 0x00 for the six bytes.

 

The setup is placed on my desk, I'm not moving it while I'm making the trials, but the direct acc and gyro readings are coherent with that (1G on the z axis, near 0 on the others and small values for the gyro) and no other code is being executed

 

Any help will be appreciated!

 

Regards,

Álvaro

 

11 replies

Federica Bossi
Technical Moderator
November 20, 2023

Hi @amarco ,

You can look at our PID examples on Github. You can find several examples about the use of the FIFO.

Hope this helps.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
amarcoAuthor
Associate
November 20, 2023

Hi Federica,

 

Yes, that is the exact code I used to enable the FIFO, but can't get any data... I have tested the code on another board to discard an IMU malfunction, but I get the same behaviour, so I guess I missing something when configuring the FIFO.

 

Regards,

Álvaro

Federica Bossi
Technical Moderator
November 21, 2023

Hi @amarco ,

Have you tried to acquire the outputs not using the FIFO?

Just to exclude problems related to your hardware.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
amarcoAuthor
Associate
November 21, 2023

Hi Federica,

 

Yes, I can get the acc and gyro readings without issues

 

Regards,

Álvaro

amarcoAuthor
Associate
November 28, 2023

Hi, any update on this? Can someone verify wether the sample code on https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dsox_STdC/examples/lsm6dsox_fifo.c actually works?

Regards,

Álvaro

kyrreaa
Associate III
January 27, 2025

I know this is old, but in case anyone sees this later:
I found that without setting ODR for XL/GYR it does not generate any data to put into FIFO. This could explain the missing data. The two settings seem independent but the ODR turns on/off the internal hardware. I do not know why the design is like this and I can not find any good explanation in the documentation but unless ODR_XL and ODR_ACC is not set to power down there is no data for FIFO.

amarcoAuthor
Associate
January 27, 2025

Hi Kirreaa,

 

Still alive, thanks for the update!

You mean that the procedure for enabling the FIFO should be as this (end part)?

 

 lsm6dsox_reset_set(&imu_dev, PROPERTY_ENABLE);
 uint8_t rst;
 do {
 lsm6dsox_reset_get(&imu_dev, &rst);
 } while (rst);

 /* Disable I3C interface */
 lsm6dsox_i3c_disable_set(&imu_dev, LSM6DSOX_I3C_DISABLE);
 /* Enable Block Data Update */
 lsm6dsox_block_data_update_set(&imu_dev, PROPERTY_ENABLE);
 /* Set full scale */
 lsm6dsox_xl_full_scale_set(&imu_dev, LSM6DSOX_2g);
 lsm6dsox_gy_full_scale_set(&imu_dev, LSM6DSOX_2000dps);
 /*
 * Set FIFO watermark (number of unread sensor data TAG + 6 bytes
 * stored in FIFO) to 10 samples
 */
 lsm6dsox_fifo_watermark_set(&imu_dev, 10);
 /* Set FIFO batch XL/Gyro ODR to 12.5Hz */
 lsm6dsox_fifo_xl_batch_set(&imu_dev, LSM6DSOX_XL_BATCHED_AT_12Hz5);
 lsm6dsox_fifo_gy_batch_set(&imu_dev, LSM6DSOX_GY_BATCHED_AT_12Hz5);
 /* Set FIFO mode to Stream mode (aka Continuous Mode) */
 lsm6dsox_fifo_mode_set(&imu_dev, LSM6DSOX_STREAM_MODE);
 /* Enable drdy 75 μs pulse: uncomment if interrupt must be pulsed */
 //lsm6dsox_data_ready_mode_set(&imu_dev, LSM6DSOX_DRDY_PULSED);
 /* Uncomment if interrupt generation on Free Fall INT1 pin */
// lsm6dsox_pin_int1_route_t int1_route;
// lsm6dsox_pin_int1_route_get(&imu_dev, &int1_route);
// int1_route.fifo_th = PROPERTY_ENABLE;
// int1_route.fifo_full = PROPERTY_ENABLE;
// int1_route.fifo_ovr = PROPERTY_ENABLE;
// int1_route.fifo_bdr = PROPERTY_ENABLE;
// lsm6dsox_pin_int1_route_set(&imu_dev, int1_route);
 /* Uncomment if interrupt generation on Free Fall INT2 pin */
// lsm6dsox_pin_int2_route_t int2_route;
// lsm6dsox_pin_int2_route_get(&imu_dev, NULL, &int2_route);
// int2_route.fifo_th = PROPERTY_ENABLE;
// int2_route.fifo_bdr = PROPERTY_ENABLE;
// int2_route.fifo_full = PROPERTY_ENABLE;
// int2_route.fifo_ovr = PROPERTY_ENABLE;
// lsm6dsox_pin_int2_route_set(&imu_dev, NULL, int2_route);
 /* Set Output Data Rate */
// lsm6dsox_xl_data_rate_set(&imu_dev, LSM6DSOX_XL_ODR_12Hz5); WRONG?
// lsm6dsox_gy_data_rate_set(&imu_dev, LSM6DSOX_GY_ODR_12Hz5); WRONG?

 lsm6dsox_xl_data_rate_set(&imu_dev, LSM6DSOX_XL_ODR_OFF); // RIGHT?
 lsm6dsox_gy_data_rate_set(&imu_dev, LSM6DSOX_GY_ODR_OFF); // RIGHT?

 

 

I have tried this with my old setup but it doesn't worked (although I didn't remember well all the details...)

 

Regards,

Álvaro

kyrreaa
Associate III
January 27, 2025

Sorry, I did not see that you had enabled the XL and GYR rates. I thought you had just selected rates for the FIFO (as this was what I had done and then it did not work).

For readout triggering I use the int1 routing of FIFO TH and it works for me.
I read the length of fifo as you do and then I read the number of samples indicated * 7 and decode each element based on the tag.

What I found useful was making sure the batch interval/watermark matched up with the ratio for accellerometer and gyro. Since I run the accelerometer faster than gyro (208Hz vs 26Hz) I have a 8:1 ratio here. So I set my watermark to 9. This gives me 8 acc + 1 gyr for every interrupt.

With equal value for acc/gyr and setting of 10 you should be getting 5 of each.

Maybe it is the order of operations?

I first always restore default configuration. Then I disable I3C and enable block updates.
Then I configure the watermark and batch rates first, before enabling both the acc and gyro by setting their rates to not powerdown. Finally I enable fifo batching by changing it from bypass mode to stream mode.

Try moving the lsm6dsox_xl_data_rate_set / lsm6dsox_gy_data_rate_set calls to enable them over the stream mode fifo call?

amarcoAuthor
Associate
January 27, 2025

Hi Kyrreaa,

I also misunderstood you and tough you had shutdown the ODR_XL and ODR_GY, but then the correct is enable ODR_XL/GYR and BATCH_XL/GYR.

The order I followed is the same on the git hub example, which is pretty much the same you are using (although you said that you enable the fifo batching in the last step).

I tried the same sequence (reset, ic3_disable, block_data_update, watermark, batch_set, scale+odr_set, fifo_mode_set_stream) but still get stuck in the loop

while (!wmflag) {
 lsm6dsox_fifo_wtm_flag_get(&imu_dev, &wmflag);
}

And if I bypass the loop, the lsm6dsox_fifo_data_level_get(&imu_dev, &fifo_num_samples) return there is no samples in the FIFO, which is consistent with no watermark_flag being triggered

Maybe is something related with the interruption :\

Did you also tried check the watermark_flag?

 

Regards,

Álvaro

kyrreaa
Associate III
January 27, 2025

I just thought of something, since I use BDU mode (block data update) it is important I always read Status1 and then Status2 so that I get updated information. Your function lsm6dsox_fifo_wtm_flag_get() does only read status2 if it is implemented identical to the sample code I was supplied. Since you do not enable BDU I am not sure if this matters.

kyrreaa
Associate III
January 27, 2025

I never check the WTM flag as I use a level interrupt on the int1 pin. When I get the interrupt I disable it and trigger reading of data. Once the reading is done I re-enable my local int1 interrupt and if the level is still high this triggers a new read immediately.

I did find an interesting line in the appnote though:
"The selected batch data rate must be equal to or lower than the output data rate
configured through the ODR_XL and ODR_G fields of the CTRL1_XL and CTRL2_G registers."

This explains why I had issues before. The ODR dictates the actual rate the system works at, and the batching rates will decimate the data from this.

amarcoAuthor
Associate
January 27, 2025

Hi Kyrreaa,

 

I though block_data_update applies only to the updates in the acc and gyro readings, but I tried

As you said, the lsm6dsox_fifo_wtm_flag_get() reads only status2, and I added a prior call for reading status1 reg

 

 while (!wmflag) {
 lsm6dsox_read_reg(&imu_dev, LSM6DSOX_FIFO_STATUS1, &wmflag, 1);
 lsm6dsox_fifo_wtm_flag_get(&imu_dev, &wmflag);
 }

 

but no luck... I also had configured the batch data rate and the output data rate at the same frequency, so I guess that it's ok

I think the problem is "turning on the FIFO", and maybe it's mandatory to use the interrupt. I'll try to explore that way, although it will require a closer look on the code from my side. But at least, I know some one was able to get the FIFO working...!

Regards,

Álvaro

kyrreaa
Associate III
January 27, 2025

Yes, the FIFO absolutely does work.
Since my code is doing so much other stuff I can't be polling the flags, thus I never tried that.
I'll add a check for the flag to see what state it is in before and after reading the data. Just to see.

I have searched for errata just to be sure but have not found any public document about it.