Skip to main content
FKara.3
Associate III
February 16, 2023
Solved

Hello, There is a Machine learning core with exportable features and filters for AI applications in LSM6DSV16X. can we use this feature by using ESP32?

  • February 16, 2023
  • 2 replies
  • 925 views

..

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome, @FKara.3​, to the community!

    You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.

    Does it answer your question?

    Regards

    /Peter

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    February 17, 2023

    Welcome, @FKara.3​, to the community!

    You should be able to use this function with all MCUs, because the MLC (Machine Learning Core) and the FSM (Finite State Machine) are integrated in the sensor and only need to be configured accordingly. You can find repositories for this under the above mentioned URLs.

    Does it answer your question?

    Regards

    /Peter

    FKara.3
    FKara.3Author
    Associate III
    February 17, 2023

    Hello Peter,

    Thank you for the answer. Yes, that was what I was looking for.

    Kindly,

    Fehmi