Skip to main content
ZHaid.1
Associate II
October 14, 2022
Question

Hi, I am trying to bring LIS3MDL to power-down mode. I have set MD Bits to 2 of "ctrl_reg3" but still, current consumption is 1-1.5mA. I have attached a schematic of LIS3MDL . Any help in this regard would be appreciated.

  • October 14, 2022
  • 2 replies
  • 1459 views

0693W00000Uo2f6QAB.png

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    October 24, 2022

    Hi @ZHaid.1​ ,

    how many LIS3MDL are you seeing behaving this way?

    You might check-first the current consumption just after the device power on (MD Bits are '11' by default).

    You should also check the default configuration of the SPI pins and the INT and DRDY from application processor side: for example, the INT and DRDY default states are low, check also the SPI ones (e.g. the CS) and tray to change them, if possible, to check if you have an extra-consumption coming from these lines.

    -Eleon

    ZHaid.1
    ZHaid.1Author
    Associate II
    October 25, 2022

    how many LIS3MDL are you seeing behaving this way?

    It is occurring on all our boards

    You might check-first the current consumption just after the device power on (MD Bits are '11' by default).

    I will get back on this thing.

    You should also check the default configuration of the SPI pins and the INT and DRDY from application processor side:

    HAL_StatusTypeDef ret = HAL_OK;

     hspi->Instance = SPI3;

     hspi->Init.Mode = SPI_MODE_MASTER;

     hspi->Init.Direction = SPI_DIRECTION_2LINES;

     hspi->Init.DataSize = SPI_DATASIZE_8BIT;

     hspi->Init.CLKPolarity = SPI_POLARITY_HIGH;

     hspi->Init.CLKPhase = SPI_PHASE_2EDGE;

     hspi->Init.NSS = SPI_NSS_SOFT;

     hspi->Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;

     hspi->Init.FirstBit = SPI_FIRSTBIT_MSB;

     hspi->Init.TIMode = SPI_TIMODE_DISABLE;

     hspi->Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

     hspi->Init.CRCPolynomial = 7;

     hspi->Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

     hspi->Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

     if (HAL_SPI_Init(hspi) != HAL_OK)

     {

       ret = HAL_ERROR;

     }

     __HAL_SPI_ENABLE(hspi);

    /* Configure LIS3MDL Interrupt Pin */

    /* PF9 */

    BSP_LIS3MDL_INT_GPIO_CLK_ENABLE();

    GPIO_InitStruct.Pin = BSP_LIS3MDL_INT_PIN;

    GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    HAL_GPIO_Init(BSP_LIS3MDL_INT_PORT, & GPIO_InitStruct);

    /* EXTI interrupt init*/

    /* Enable and set EXTI Interrupt priority */

    HAL_NVIC_SetPriority(BSP_LIS3MDL_INT_EXTI_IRQn, BSP_LIS3MDL_INT_EXTI_IRQ_PP, BSP_LIS3MDL_INT_EXTI_IRQ_SP);

    HAL_NVIC_EnableIRQ(BSP_LIS3MDL_INT_EXTI_IRQn);

    /* Configure LIS3MDL Data Ready Pin */

    /* PC8 */

    BSP_LIS3MDL_DR_GPIO_CLK_ENABLE();

    GPIO_InitStruct.Pin = BSP_LIS3MDL_DR_PIN;

    GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    HAL_GPIO_Init(BSP_LIS3MDL_DR_PORT, & GPIO_InitStruct);

    For example, the INT and DRDY default states are low, check also the SPI ones (e.g. the CS)

    Pin Status when device starts:

    Status of BSP_LIS3MDL_INT_PIN = 0

    Status of BSP_LIS3MDL_DR_PIN = 0

    Status of BSP_LIS3MDL_CS_PIN = 1

     

    Pin status in continuous mode:

    Status of BSP_LIS3MDL_INT_PIN = 0

    Status of BSP_LIS3MDL_DR_PIN = 1

    Status of BSP_LIS3MDL_CS_PIN = 1

     

    Pin status in power down mode:

    Status of BSP_LIS3MDL_INT_PIN = 0

    Status of BSP_LIS3MDL_DR_PIN = 0

    Status of BSP_LIS3MDL_CS_PIN = 1