Skip to main content
CWell.1
Visitor II
January 24, 2023
Question

How to configure LSM6DS3 inactivity / activity capabilities

  • January 24, 2023
  • 1 reply
  • 1016 views

Hello,

I was trying to setup an inactivity/activity program in Arduino using a Xiao Sense NRF52840, that has the LSM6DS3 chip on it, and with using the register i was trying to recognize inactivity and activity. If anyone has insight as to why this isnt working it would be appreciated.

#include "LSM6DS3.h"
#include "Wire.h"
 
#define CLEAR_STEP true
#define NOT_CLEAR_STEP false
 
//Create a instance of class LSM6DS3
LSM6DS3 lsm6ds3(I2C_MODE, 0x6A); //I2C device address 0x6A
uint16_t detectCount = 0;
 
void setup() {
 Serial.begin(9600);
 while (!Serial);
 if (lsm6ds3.begin() != 0) {
 Serial.println("Device error");
 } else {
 Serial.println("Device OK!");
 }
 
 if (0 != config_free_fall_detect()) {
 Serial.println("Fail to configure!");
 } else {
 Serial.println("Success to Configure!");
 }
}
 
void loop() {
 uint8_t readDataByte = 0;
 //Read the wake-up source register
 lsm6ds3.readRegister(&readDataByte, LSM6DS3_ACC_GYRO_WAKE_UP_SRC);
 //Mask off the FF_IA bit for free-fall detection
 readDataByte &= 0x10;
 if (readDataByte) {
 detectCount ++;
 Serial.print("Inactivity Detected! ");
 Serial.println(detectCount);
 }
 delay(10);
}
 
int config_free_fall_detect(void) {
 uint8_t error = 0;
 uint8_t dataToWrite = 0;
 
 dataToWrite |= LSM6DS3_ACC_GYRO_BW_XL_200Hz;
 dataToWrite |= LSM6DS3_ACC_GYRO_FS_XL_2g;
 dataToWrite |= LSM6DS3_ACC_GYRO_ODR_XL_416Hz;
 
 error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_CTRL1_XL, dataToWrite);
 error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_WAKE_UP_DUR, 0x42);
 error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_WAKE_UP_THS, 0x42);
 error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_MD1_CFG, 0x80);
 
 return error;
}

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    Technical Moderator
    April 11, 2023

    Hi @CWell.1​ ,

    Welcome to ST Community!

    After WAKE_UP_THS you need to write E0h to TAP_CFG.


    _legacyfs_online_stmicro_images_0693W00000bhr6pQAA.pngLet me know if this works!

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.