Skip to main content
JasonRrrr
Associate II
April 11, 2024
Question

i2c address selection leakage current with 2 x LIS2DW12 on one PCB

  • April 11, 2024
  • 1 reply
  • 851 views

I want to use 2x LIS2DW12 accelerometers on one PCB.

I used i2c to save GPIOs.

The i2c address is selected by pulling the SDO/SAO pin HIGH or LOW and it is internally pulled HIGH with approximately 20kohm at 3.6v.

If I just connect it to GND then I can expect 180uA leakage.

If I use a resistor to pull it down then I calculate that to get a LOW value of 0.2 x 3.6v (0.72V) I need to use a pull down of at least 5Kohms. But this implies a leakage current of 146uA. Which is still not great.

Is there another way to connect 2 x LIS2DW12, except using SPI? 

Can I connect the SDO/SAO to a GPIO and toggle it LOW when I want to read either accelerometer, and leave it floating the rest of the time? (pulled high)

 

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
April 30, 2024

Hi @JasonRrrr ,

Yes, it is possible to toggle the SA0  by GPIO to have the LOW-Address only for the sensor read. But the other sensor address should be HIGH and not floating.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.