Skip to main content
Associate II
January 16, 2026
Question

I2C bus lockup (SDA held low) involving ISM330 and IIS2MDC

  • January 16, 2026
  • 2 replies
  • 342 views

Problem description:

We are seeing a hard I2C bus lockup involving an ISM330 IMU and an IIS2MDC magnetometer on the same bus.

 

The failure mode is that SDA is driven low permanently, and the bus cannot be recovered by standard I2C recovery procedures (9–20 SCL pulses with SDA released).

 

This occurs both immediately after MCU firmware is flashed and during nominal runtime, seemingly at random.

 

Once the condition occurs, a full MCU reset does not recover the bus. On a bench setup we confirmed by probing that SDA is physically held low.

 

Hardware configuration:

MCU: STM32 acting as I2C master

Devices on bus:

  • ISM330 (IMU)
  • IIS2MDC (magnetometer)

These are the only slaves on the bus.

Standard I2C pull-ups are used, with no level shifting.

 

I've done additional testing to try to find the problematic device by removing devices and reconfiguring connections (auxiliary I2C), see results below.

 

Observed behavior by configuration:

  • ISM330 only on I2C: no issues
  • ISM330 and IIS2MDC directly on MCU I2C: SDA eventually stuck low and not recoverable
  • IIS2MDC only on I2C: no issues
  • ISM330 and IIS2MDC via auxiliary I2C (SDx and SCx): same failure occurs, but sometimes recoverable by clocking

During failure, probing shows both main SDA and SDx (when using auxiliary I2C) are held low

 

In the direct-connection case, forced SCL clocking (9–20 pulses) does not release SDA.

In the auxiliary I2C case, forced clocking sometimes recovers the bus, but the fault still occurs.

 

Key observation:

  • Based on the testing, having the combination of both devices directly on the I2C bus causes lock up.
  • Neither of the devices alone ever locks up the bus.
  • When both devices are present, the bus can be locked up until devices are power cycles.

 

Questions for ST engineering:

  1. Is IIS2MDC known to hold SDA low under any fault condition such as mid-transaction reset, brownout, internal state machine stall, or clock stretching related issues?
  2. What exactly does the ISM330 sensor hub do on SDx when a downstream slave is stuck? Does it actively generate clocks, reset the I2C state machine, or tri-state the SDx line?
  3. Is auxiliary I2C expected to be more tolerant of a misbehaving slave than direct I2C connection?
  4. Is there a documented or recommended recovery sequence, such as register writes, reset commands, or power cycling order, to force IIS2MDC to release SDA once it is stuck?

2 replies

TDK
Super User
January 16, 2026

Look at the SDA/SCL on a logic analyzer and see what happens when SDA gets stuck low.

CS lines are driven high?

SCL line remains free when SDA is stuck low?

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
L-liAuthor
Associate II
January 16, 2026

CS lines are driven high?


CS lines are pulled high in the circuit.


SCL line remains free when SDA is stuck low?


SCL line is free when SDA is stuck low. As mentioned in the post, I've also tried clock it out in the direct I2C configuration with no luck but with the aux I2C configuration it was able to recover.

Anything I should try and test?

TDK
Super User
January 16, 2026

I think you need a logic analyzer to see what's going on. Slaves are not allowed to hold 0 on SDA indefinitely. What is the bus master?

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Super User
January 17, 2026

Maybe I could have been more clear. I meant looking at the bus at the time SDA becomes stuck. The hope is that you can identify an event or transaction or some other bus error that causes the issue. And see if that is repeatable. Even if the master is not holding SDA low, it may be doing something it shouldn't to cause the slave to misbehave.

> The bus master is a STM32

It would be helpful to be more specific. There are many different families with a handful of different I2C implementations among them. Some of these families have I2C related errata.

"If you feel a post has answered your question, please click ""Accept as Solution""."
L-liAuthor
Associate II
January 20, 2026

OK thanks for clarifying that, I'll work on recreating the issue and getting a scope trace.


It would be helpful to be more specific. There are many different families with a handful of different I2C implementations among them. Some of these families have I2C related errata.


The STM32H723ZG, lmk if you need more detail.