Skip to main content
JOmbe.2
Associate
February 6, 2023
Question

IIS2DLPC not responding via SPI, wrong component or issue with communication?.

  • February 6, 2023
  • 1 reply
  • 686 views

Hi,

We have received a new batch of boards and the sensor is not responding (The only change is the solder mask colour) to the "Who_am_I_ID" command. In the previous batch every thing worked as intended.

Is it possible to, based on QR code, to see if these two chips are the same component, see images below? When measuring the SPI communication, the clock and MOSI seems OK, but the MISO signal is ~1.5V and is not responding. On the working board the signal is either 3V or 0V.

What could be the issue?

 0693W00000YA5D6QAL.pngBR

Johannes

    This topic has been closed for replies.

    1 reply

    JOmbe.2
    JOmbe.2Author
    Associate
    February 7, 2023

    Read out of the QR code:

    Old board: 781050DE02FN042

    Another old board: 781050DE02FO0UV

    The new non-working board: 781050DE02FL23J

    It seems like the same circuit, but could anyone confirm?