Skip to main content
ACand.3
Associate III
February 7, 2025
Question

Inactivity Mode for the lsm6dsv16x IMU

  • February 7, 2025
  • 1 reply
  • 552 views

Hello there, 

 

Are there any examples on how to use the inactivity feature of the lsm6dsv16x?

I checked the github and I only see for waking up, but not the other way around.

 

My goal is to set a device to sleep once there is no motion from imu. meaning, once the imu has no motion, it sets an interrupt like hey there is no motion going on, go to sleep/off mode. 

Then once there is motion, I want the imu to fire a interrupt telling device, here wake up. 

Is it possible to use one Interrupt pin for both cases or do I need to use both?


1 reply

Andrea VITALI
ST Employee
February 21, 2025

Check app note AN5763 paragraph 5.6 for activity/inactivity embedded logic and how to configure it and route the corresponding interrupts to the dedicated pins.

Here is some high-level note:

  • wake-up logic generates the interrupt when motion is detected (the absolute value of any axis is above the programmed threshold for the minimum programmed time)
  • activity/inactivity logic not only generates interrupts but also changes the device configuration! during inactivity the device switches to low-power mode at low ODR save power, during activity power mode and ODR are restored as they were before
  • stationary/motion logic is the same as activity/inactivity but without any change in power mode and ODR

You probably need to configure and use stationary/motion logic right?