Skip to main content
Visitor II
June 10, 2025
Solved

Is LSM6DSL zephyr driver compatible with LSM6DSR ?

  • June 10, 2025
  • 2 replies
  • 376 views

Hi,

 

I am trying to create test the STEVAL-MKI194V1 for a test vehicle, which has LSM6DSR. However, I do not get an initialization response from it using the Zephyr device tree. So, I did a test (without the DSL driver) with the spi shell which gives me the correct chip ID output. Is the DSL driver compatible with the DSR? OR would I need a separate driver for both ? 

 

Thanks,

 

Devang 

 

 

Best answer by Federica Bossi

Hi @devangs33 ,

You should use the LSM6DSR driver.

2 replies

Federica Bossi
Federica BossiBest answer
Technical Moderator
June 12, 2025

Hi @devangs33 ,

You should use the LSM6DSR driver.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Billy OWEN
ST Employee
June 13, 2025

Hi @devangs33 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy