Skip to main content
Associate
September 8, 2023
Solved

ism330dlc: Change of Accelerometer full-scale selection during operation

  • September 8, 2023
  • 2 replies
  • 2680 views

Hey, 

i am currently planning to work with the ISM330DLC and am wondering if its possible to change the full-scale selection of Accelerometer (CTRL1_XL (10h) - FS_XL [1:0]during operation. Or is it mandatory to stop the ISM to change the control register values. I could not find any  information regarding that topic in the datasheet attached.

 

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @st_ks ,

Welcome to ST Community!

You can change the FS while the device is working.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

2 replies

jiangfan
ST Employee
September 8, 2023

Just try it.

I mean you may try to change the full-scale selection of Accelerometer, to see if it works as you expected. I suppose it is easy to try - just display/print current full-scale + current raw value + current Acceleration value.

Federica Bossi
Federica BossiBest answer
Technical Moderator
September 8, 2023

Hi @st_ks ,

Welcome to ST Community!

You can change the FS while the device is working.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
st_ksAuthor
Associate
September 11, 2023

Hi, that means I can change the "full-scale selection" as often as the communication via SPI or I2C allows?