Skip to main content
Associate
February 5, 2025
Solved

ISM330DLC FIFO AXL+Gyro+Timestamp

  • February 5, 2025
  • 3 replies
  • 2455 views

Dear Support
I want to add timestamp registration to the FIFO.
I already use FIFO to save gyroscope and accelerometer samples, but I'm struggling to add timestamps.
Since ODR is too high for polling mode the only solution is this one.
I attach some code snippets to make it clear, also consider them as pseudo code taken from a more complex structure.
ism330dlc_fifo_time_set and timer_rd are not present in the library but I wrote them based on the AN5125

 

int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
	ism330dlc_fifo_ctrl2_t fifo_ctrl2;
	int32_t ret;
	ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2,
							 1);
	if (ret == 0) {
		fifo_ctrl2.fifo_timer_en = val;
		ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2,
								 (uint8_t *)&fifo_ctrl2, 1);
	}

	return ret;
}​
uint64_t ism330dlc_timer_rd(stmdev_ctx_t *ctx) {
	uint64_t time = 0;
	uint8_t t0;

	ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP0_REG, (uint8_t *)&t0, 1);

	time = t0;
	ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP1_REG, (uint8_t *)&t0, 1);
	time |= uint64_t(t0 << 8);
	ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP2_REG, (uint8_t *)&t0, 1);
	time |= uint64_t(t0 << 16);

	return time * 25;
}
void start_routine() {		
 sens.freq = 104u;
		pattern_len = 18;

		ism330dlc_block_data_update_set(&ctx.Ctx, PROPERTY_ENABLE);

		ism330dlc_int1_route_t int_1_reg{};
		ism330dlc_pin_int1_route_get(&ctx.Ctx, &int_1_reg);
		int_1_reg.int1_fth = PROPERTY_ENABLE;
		ism330dlc_pin_int1_route_set(&ctx.Ctx, int_1_reg);
		ism330dlc_fifo_watermark_set(&ctx.Ctx, sens.freq * pattern_len);

 		ISM330DLC_ACC_Enable(&ctx);
		ISM330DLC_GYRO_Enable(&ctx);
		ISM330DLC_ACC_SetOutputDataRate(&ctx, sens.freq);
		ISM330DLC_GYRO_SetOutputDataRate(&ctx, sens.freq);
		ism330dlc_fifo_dataset_4_batch_set(&ctx.Ctx, ISM330DLC_FIFO_DS4_NO_DEC);
		ism330dlc_fifo_xl_batch_set(&ctx.Ctx, ISM330DLC_FIFO_XL_NO_DEC);
		ism330dlc_fifo_gy_batch_set(&ctx.Ctx, ISM330DLC_FIFO_GY_NO_DEC);

		ism330dlc_timestamp_res_set(&ctx.Ctx, ISM330DLC_LSB_25us);
		// ism330dlc_timer_int_set(&ctx.Ctx, 1);

		ism330dlc_timestamp_set(&ctx.Ctx, 1);

		ism330dlc_fifo_time_set(&ctx.Ctx, 1);

		ISM330DLC_FIFO_Set_ODR_Value(&ctx, sens.freq);
		ism330dlc_fifo_mode_set(&ctx.Ctx, ISM330DLC_STREAM_MODE);​
}

void loop(){
 int16_t num;
	ism330dlc_fifo_data_level_get(&ctx.Ctx, &num);
		
		for (auto i = 0u; i < num; i++) {
			uint16_t pat;
			axis ax[3]{};

			ism330dlc_fifo_pattern_get(&ctx.Ctx, &pat);
			auto &v = ax[pat / 3].ax.i16bit[pat % 3];
			ism330dlc_fifo_raw_data_get(&ctx.Ctx, (uint8_t *)&v, sizeof(v));
			auto m = (pat < 3) ? sens.gy / 1000
					 : pat < 6 ? sens.axl / 1000
							 : 25;
			auto e = su::stringify(float(v) * m, 2);
			auto tm = ism330dlc_timer_rd(&ctx.Ctx);
			slog::println("IMU", [&]() {
				return su::stringify(tm) + " pat " + su::stringify(pat) + " " +
					 e;
			}());
		}
}

 

 

Notes:
- trying different ODRs makes the same results
- enabling/disabling BDU won't change anything

- Loop() is called in a task when the IRQ is triggered

 

 

These are the results:
Gyro and accelerometer data are well converted, but I always read 0 to pattern 6-7-8, even if I can read timestamp registers correctly.

results: Timestamp in polling + #pattern + converted gy/axl and zero timestampresults: Timestamp in polling + #pattern + converted gy/axl and zero timestamp
Looking forward to hearing from you,
Best regards,
Andrea

Best answer by andross092

I opened this pull request
https://github.com/STMicroelectronics/stm32-ism330dlc/pull/2 
The problem was there so this fixed the issue

3 replies

Federica Bossi
Technical Moderator
February 6, 2025

Hi @andross092 ,

To add timestamp registration to your FIFO data, you can follow these steps:

  1. Enable the FIFO timestamp feature: This is done by setting the appropriate bits in the FIFO control registers.
  2. Read the timestamp values: Each time you read data from the FIFO, also read the corresponding timestamp.

Try these functions with for the timestamp functionality:

%Function to Set FIFO Time

int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
 ism330dlc_fifo_ctrl2_t fifo_ctrl2;
 int32_t ret;
 ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2, 1);
 if (ret == 0) {
 fifo_ctrl2.fifo_timer_en = val;
 ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2, 1);
 }
 return ret;
}
%Function to Read Timer
uint64_t ism330dlc_timer_rd(stmdev_ctx_t *ctx) {
 uint64_t time = 0;
 uint8_t t0;

 ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP0_REG, (uint8_t *)&t0, 1);
 time = t0;
 ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP1_REG, (uint8_t *)&t0, 1);
 time |= uint64_t(t0 << 8);
 ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP2_REG, (uint8_t *)&t0, 1);
 time |= uint64_t(t0 << 16);

 return time * 25; // Assuming 25us resolution
}

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
February 6, 2025

Hi Federica
Thanks for your reply.
Since those were my functions and you just copied them I suppose what I'm trying to do is already correct.
But as you can see from my logs those configurations aren't working as expected, because I cannot retrieve any valid timestamp from the FIFO

Associate
February 11, 2025

Dear support,
Is there any update on the topic?

Andrea VITALI
ST Employee
February 26, 2025

Did you set the batch data for batch #4 dedicated to timestamps? 

ism330dlc_fifo_dataset_4_batch_set()

Then looking at the AN5125 it seems that bit #7 (128) must be set in FIFO_CTRL2 to enable the timestamps in batch #4 (you seem to set bit #0)

The corresponding function does not exist in the official driver on GitHub, but one can copy rename and change the similar function ism330dlc_fifo_temp_batch_set() that enables temperature in batch #4

let us know if this solves

Associate
February 27, 2025

HI Andrea,
Thanks for your reply.
I actually set that bit to one in this function

int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
	ism330dlc_fifo_ctrl2_t fifo_ctrl2;
	int32_t ret;
	ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2,
							 1);
	if (ret == 0) {
		fifo_ctrl2.fifo_timer_en = val;
		ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2,
								 (uint8_t *)&fifo_ctrl2, 1);
	}

	return ret;
}

 when I call 

		ism330dlc_fifo_time_set(&ctx.Ctx, 1);

in the init
but since you highlighted the fact that is the 7th bit I guess I have an answer:

Take a look at ism330dlc_reg.h:

andross092_0-1740666903702.png

this struct splits register in 9bit instead of 8, so I don't know where I'm actually writing

andross092AuthorBest answer
Associate
February 27, 2025

I opened this pull request
https://github.com/STMicroelectronics/stm32-ism330dlc/pull/2 
The problem was there so this fixed the issue

Andrea VITALI
ST Employee
February 27, 2025

glad we found the issue!