Skip to main content
Visitor II
December 31, 2025
Question

Linux I3C Slave Driver with IBI Support for LSM6DSO

  • December 31, 2025
  • 1 reply
  • 321 views

Hello,

My goal is to test the IBI functionality of my custom I3C master driver using the LSM6DSOX sensor. For this test, I need the Linux I3C slave driver for LSM6DSOX with IBI support. The file linux/driver/iio/imu/st_lsm6dx/st_lsm6dsx_core.c does not contain any IBI-related code, such as i3c_device_request_ibi. If anyone has an example or code for using IBI with I3C in a Linux environment, could you please share it?.

 

1 reply

Federica Bossi
Technical Moderator
February 2, 2026

Hi @MinKi ,

There is currently no Linux IIO driver for LSM6DSOX that uses I3C IBI from ST.

You could use an existing I3C IBI‑enabled driver as a reference and extend the LSM6DSOX driver.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.