Skip to main content
Associate
September 25, 2023
Question

LIS2DE12 - Sleep to Wake Function

  • September 25, 2023
  • 1 reply
  • 1058 views

Hello,

I'm looking to see if there is a maximum value for the sleep-to-wake interrupt register on the LIS2DE12. I do see +/- 2g, 4g, 8g, 16g as standard values, but is it okay to set a threshold value to +/-30g, 25g or 20g?

Thanks!

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
September 28, 2023

Hi @baraadalaq ,

Welcome to ST Community!

You need to stay within the FS range, so at maximum value of 16g.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
September 29, 2023

Thanks for the reply. Would the device become unstable past the maximum value?