Skip to main content
Smalik
Associate III
January 17, 2023
Question

LIS2DH12TR- Not working on 2.9V and above voltages

  • January 17, 2023
  • 1 reply
  • 1100 views

Hello,

I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greater than 2.8V?

Any help would be appreciable

Thanks and Regards

Sarthak Malik

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    January 17, 2023

    Hi @Smalik​ ,

    let's keep only this thread active.

    -Eleon