Skip to main content
Associate
November 13, 2025
Question

LIS2DU12 wake up configuration

  • November 13, 2025
  • 2 replies
  • 213 views

Hi everyone,

I'm using 2 LIS2DU12 on one object.

The first one is configured in continuous mode. I forward the samples directly to a computer. I use it to check the wake up triggering configuration of the second one.

The second one is configured in continuous-to-FIFO mode. And I'm trying to get it to wake up when the acceleration on one axis is over 2g for at least 8.75ms. ODR is 800Hz, FS=16g, so I set :

WK_THS=8
WAKE_THS_W=0
=> threshold = 2g x 2⁶ / 16g = 8

WAKE_DUR=01 (7 ODR_time)
WU_DUR_X4=1
=> Wake-up duration = 7 / 800 = 8.75ms

The first LIS2DU12 configured in continuous mode shows that during my tests I get 4g for over 20ms, yet the second LIS2DU12 does not wake up. But if I set the threshold to 4 (i.e. 1g according to my calculations) it does wake up, and I recover 2 very similar acquisitions.

What did I misunderstand ?

Here is a code snippet of the configuration of the LIS2DU12 in continuous-to-FIFO mode:

 
 lis2du12_pin_int_route_t int_route;
 lis2du12_status_t status;
 lis2du12_id_t id;

 /* Initialize mems driver interface */
 dev_ctx.write_reg = spi_write;
 dev_ctx.read_reg = spi_read;
 dev_ctx.mdelay = platform_delay;
 dev_ctx.handle = p_bus;

 /* Wait sensor boot time */
 platform_delay(BOOT_TIME);

 /* Check device ID */
 lis2du12_id_get(&dev_ctx, &id);
 if (id.whoami == LIS2DU12_ID)
 {
 printf("-Part ID: 0x%02X\r\n", id.whoami);
 }
 else
 {
 printf("Echec Lecture ID...\r\n");
 }

 /* Restore default configuration */
 lis2du12_init_set(&dev_ctx, LIS2DU12_RESET);
 do {
 lis2du12_status_get(&dev_ctx, &status);
 } while (status.sw_reset);


 /* Set bdu and if_inc recommended for driver usage */
 lis2du12_init_set(&dev_ctx, LIS2DU12_DRV_RDY);


 // Configure CTRL 5 en power down
 md.odr = LIS2DU12_OFF;
 lis2du12_mode_set(&dev_ctx, &md);

 // configure mode Wake up
 // Activer la détection sur X, Y et Z
 wkup_md.x_en = 1;
 wkup_md.y_en = 1;
 wkup_md.z_en = 1;
 wkup_md.threshold = 8; // Thres=±2g, FS=±16g, 1LSB of thres=FS/2^6 => 2g*2⁶/16g=2³
 wkup_md.duration = 5; // 5 => WU_DUR_X4=1 & WAKE_DUR=1 => duration=7 ODR_time =7/800Hz=8,75ms
 wkup_md.sleep.en = 0;
 lis2du12_wake_up_mode_set(&dev_ctx,&wkup_md);


 /* Select bus interface */
 lis2du12_bus_mode_set(&dev_ctx, LIS2DU12_I3C_DISABLE);

 /* Set FIFO watermark to 64 sample(s) */
 fifo_mode.store = LIS2DU12_8_BIT;
 fifo_mode.watermark = 64;
 fifo_mode.operation = LIS2DU12_STREAM_TO_FIFO;
 lis2du12_fifo_mode_set(&dev_ctx, &fifo_mode);


 // CONFIGURE CTRL 5 en 16g et ODR de 800Hz
 /* Set Output Data Rate */
 md.fs = LIS2DU12_16g;
 md.odr = LIS2DU12_800Hz;
 lis2du12_mode_set(&dev_ctx, &md);


 /* Configure interrupt pins */
 lis2du12_pin_int2_route_get(&dev_ctx, &int_route);
 int_route.wake_up = PROPERTY_ENABLE;
 lis2du12_pin_int2_route_set(&dev_ctx, &int_route);

 

2 replies

Federica Bossi
Technical Moderator
November 13, 2025

Hi @Ch4rly ,

Some suggestions:

  • Try setting wkup_md.duration = 1; to have 7 ODR cycles duration with WU_DUR_X4=1.
  • Explicitly set the WU_DUR_X4 bit: if the driver does not set it automatically, write directly to the MD1_CFG (0x1F) register bit 4 (WU_DUR_X4).

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ch4rlyAuthor
Associate
November 26, 2025

Hi @Federica Bossi,

Thanks for the reply.

I checked that's what "lis2du12_wake_up_mode_set" does : WU_DUR_X4=1 and WAKE_DUR=01.

That being said. Does my calculations for

  • threshold=2G
  • wake-up duration=8.75ms

make sense to you ?

Federica Bossi
Technical Moderator
January 14, 2026

Hi @Ch4rly ,

Your calculations are ok. Please consider that wake-up function use slope filtered data (see AN5648 5.1), and threshold apply to output of internally filtered data. Also consider that Cont-to-FIFO mode can be triggered if wake-up interrupt is routed to INT1 pin (AN5648 6.4.4), which I cannot see in your code.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ch4rlyAuthor
Associate
November 17, 2025

Hi Federica,

Thanks for the reply.

I checked that's what "lis2du12_wake_up_mode_set" does : WU_DUR_X4=1 and WAKE_DUR=01.

Does my calculations make sense to you ?