Skip to main content
Associate II
November 29, 2024
Question

LIS2DW12 consumption in fifo mode

  • November 29, 2024
  • 1 reply
  • 455 views

Hello, 

I'm using the LIS2DW12 on my own board.

Consumption seems a little high to me. In the datasheet I found a value around 5.5µA and I obtained rather 45µA.The configuration is as follows:
- ODR 50Hz
- FIFO in continious mode with INT1 enabled

- Full-scale 4g

- 14 bits resolution in LP2.

I did not find any information regarding consumption in FIFO mode. Can you give me some information?

Thanks

1 reply

Federica Bossi
Technical Moderator
December 5, 2024

Hi @laesser ,

We do not expect such high consumption. When you acquire without using FIFO what consumption do you have?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.