Skip to main content
VMali.2
Associate
June 6, 2023
Solved

LIS2DW12 Current Consumption.

  • June 6, 2023
  • 2 replies
  • 1826 views

Hello STMicroelectronics Support Team,

I am currently working on a development project where I'm utilizing the LIS2DW12 accelerometer. However, I've encountered an issue with the current consumption of the accelerometer on our custom board. I would appreciate your assistance in resolving this matter.

Configuration Used:

lis2dw12_block_data_update_set(&dev_ctx1, PROPERTY_ENABLE);

lis2dw12_full_scale_set(&dev_ctx1, LIS2DW12_8g);

lis2dw12_filter_path_set(&dev_ctx1, LIS2DW12_LPF_ON_OUT);

lis2dw12_filter_bandwidth_set(&dev_ctx1, LIS2DW12_ODR_DIV_4);

lis2dw12_power_mode_set(&dev_ctx1, LIS2DW12_HIGH_PERFORMANCE);

lis2dw12_data_rate_set(&dev_ctx1, LIS2DW12_XL_ODR_25Hz);

Issue:

After incorporating the LIS2DW12 accelerometer into our custom board, we noticed a current consumption of approximately 1.5 mA. However, upon removing the accelerometer, the current consumption dropped to 1.5 uA. We expected the accelerometer to be a low-power device, and this discrepancy in current consumption has raised concerns.

Suggestions Tried:

  1. Verified that the accelerometer is operating in the low-power mode (LIS2DW12_LOW_POWER) rather than high-performance mode.
  2. Reduced the Output Data Rate (ODR) to a lower value that still meets our application requirements.
  3. Adjusted the Full Scale Range to a lower value (e.g., LIS2DW12_2g).
  4. Reviewed and considered disabling the filter path (LIS2DW12_LPF_DISABLE) to reduce power consumption.
  5. Disabled the Block Data Update feature (PROPERTY_DISABLE) if it is not required for our application.
  6. Ensured a stable and noise-free power supply to the accelerometer.

Despite these efforts, we are still experiencing higher than expected current consumption with the LIS2DW12 accelerometer.

Could you please provide us with further guidance or suggestions on how to achieve minimum current consumption with the LIS2DW12 accelerometer? We would greatly appreciate your expertise and assistance in resolving this issue.

Thank you in advance for your support.

Regards,

Vitthal.

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @Vitthal Mali​ ,

    First I suggest you to remove R4 and R5 since they are output push-pull.

    If you want to use them in open drain configuration please enable PP_OD in reg 22h.

    If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster :)

    2 replies

    Federica Bossi
    Technical Moderator
    June 6, 2023

    Hi @Vitthal Mali​ ,

    Welcome to ST Community!

    Can you please share your schematic?

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    VMali.2
    VMali.2Author
    Associate
    June 6, 2023

    Hello Federica Bossi (ST Employee)


    _legacyfs_online_stmicro_images_0693W00000bVhgyQAC.png 


    _legacyfs_online_stmicro_images_0693W00000bVhhSQAS.png 

    We encountered a situation where the same SDA and SCL pins of our NRF52833 Microcontroller are connected to both an accelerometer and a temperature sensor. During our investigation, we discovered that the CS (Chip Select) pin of the LIS2DW12 accelerometer has an internal pull-up register. As a result, we removed the R3 register and connected 4.7k pull-up resistors to the SDA and SCL lines. CS Pin of LIS2DW12 is kept open.

    We would appreciate your support in confirming whether our approach is appropriate for this configuration. Specifically, we would like to know if connecting the pull-up resistors to the shared SDA and SCL lines is a suitable solution. Additionally, we would like to ensure that this setup will not cause any conflicts or issues with the communication between the NRF52833 microcontroller and the devices connected to the shared bus.

    Regards,

    Vitthal.

    Federica Bossi
    Federica BossiBest answer
    Technical Moderator
    June 6, 2023

    Hi @Vitthal Mali​ ,

    First I suggest you to remove R4 and R5 since they are output push-pull.

    If you want to use them in open drain configuration please enable PP_OD in reg 22h.

    If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster :)

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.