Skip to main content
Visitor II
June 12, 2025
Solved

LIS2DW12 – Detecting Orientation Change in Degrees Using Interrupt

  • June 12, 2025
  • 1 reply
  • 323 views

We are using the LIS2DW12 accelerometer in our custom product. We understand that this sensor can detect movement or positioning along the X, Y, and Z axis. However, in our application, we need to detect when the device changes its orientation in terms of degrees—for example, when it flips or tilts significantly from one position to another.

Can the LIS2DW12 generate an interrupt based on such orientation changes (e.g., using 6D orientation detection)? We are looking for a way to trigger events when the device is rotated beyond a certain angle.

Thank you

Best answer by Federica Bossi

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
June 12, 2025

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.