Skip to main content
Associate
July 19, 2024
Solved

LIS2DW12 Unable to communicate through I2C

  • July 19, 2024
  • 3 replies
  • 1493 views

Hi,

 

I am using the LIS2DW12 on my board communicating over I2C with the nRF52840.  I have not yet been able to communicate with the accelerometer at all, and all attempts to read or write end the same way (see screenshot)

I have the CS and SA0 lines both pulled up to VDD, and VDDIO is tied to VDD because they are the same voltage, 1.8V.  Could there be an issue with VDD and VDDIO being the same rail? 


Best answer by cwhitelo1454

Turns out the manufacturing house used the LIS2DS12 instead of the LIS2DW12 that was on the BOM....

3 replies

Tesla DeLorean
Guru
July 20, 2024

Should work as described. Look for other causes.

Check the schematic, check the pins/orientation

Try both the (0x18<< 1) and (0x19<< 1) addresses (high order 7-bit)

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
AScha.3
Super User
July 20, 2024

Hi,

from ds

>  If the SA0/SDO pin is connected to the supply voltage, the address is 0011001b,

So use 0x32 / 0x33 (w/r) as its address .

"If you feel a post has answered your question, please click ""Accept as Solution""."
cwhitelo1454AuthorBest answer
Associate
July 23, 2024

Turns out the manufacturing house used the LIS2DS12 instead of the LIS2DW12 that was on the BOM....