Skip to main content
Associate II
November 20, 2024
Solved

LPS22DF: Polarity of INT_DRDY pin?

  • November 20, 2024
  • 1 reply
  • 586 views

I would like to change the state of the INT_DRDY of LPS22DF. I have tried to change the value of INT_H_L bit in register CTRL_REG3 (12h), but it has no (immediate) effect. Is it necessary to activate the pin? I have also tried different values in CTRL_REG4 (13h), without effect.

Thank you.

Best answer by tcachat

Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).

1 reply

tcachatAuthorBest answer
Associate II
November 20, 2024

Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).