Skip to main content
Visitor II
October 9, 2025
Question

LPS28DFW Mechanical Limit

  • October 9, 2025
  • 1 reply
  • 126 views

Hello everyone,

I plan to use the LPS28DFW barometer to measure the final pressure after a drop from 30 atm.

I only need to sense the final pressure within the sensor’s specified working range, but I’d like to know whether exposure to the initial 30 atm would cause mechanical damage to the device. Or, at what pressure can I expect the sensor to break?

Thanks!

1 reply

Federica Bossi
Technical Moderator
December 24, 2025

Hi @tom23song ,

The LPS28DFW is designed for atmospheric pressure ranges and cannot withstand pressures as high as 30 atm without likely sustaining mechanical damage. Its maximum rated pressure is far below 30 atm. For measuring pressures up to 30 atm, a dedicated high-pressure sensor should be used to avoid damaging the device.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.