Skip to main content
Visitor II
September 2, 2025
Question

LSM303AGR Application Note Clarification Needed

  • September 2, 2025
  • 1 reply
  • 560 views

Hello everyone,

I am currently using the LSM303AGR's magnetometer and accelerometer. After coding the self-test procedure from the datasheet, and noticed that the number of samples for the magnetometer self-test is way higher than the number of samples for the accelerometer self-test (5 for the Accelerometer, 50 for the Magnetometer).

When looking at the Application Note (AN4825: ultra-compact high-performance eCompass module based on the LSM303AGR), the number of samples to average is 5 at page 21/65 - Magnetometer self-test), whereas it is 50 in the next figure at page 22/65 (Figure 3. Magnetometer self-test procedure).

Which one should it be ?

Thanks in advance,

CJ

1 reply

Federica Bossi
Technical Moderator
September 11, 2025

Hi @jasoncerisier ,

Thanks for notice us.

Let me check with the team and come back to you.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.