Skip to main content
Associate II
May 16, 2025
Solved

LSM6DS, ASM330, ISM330 digitization multiplexing and filtering

  • May 16, 2025
  • 1 reply
  • 403 views

Hello,

Could you please confirm that in LSM6DS, as in ASM330, as in ISM330, the low pass gyroscope filtering LPF2 cannot be bypassed and is only driven by ODR_G (no "enable" flag is available for this filtering stage) ?  

Furthermore, the block diagrams in the corresponding datasheets suggest that a single ADC (ADC1) is used to digitize the three axes of the gyroscope. Could you please confirm that digitization is indeed multiplexed in these products ?

Thank you by advance for your help.

Best answer by Federica Bossi

Hi @fgs ,

The LPF2 is not configurable and the cutoff frequency depends on the ODR_G.

There are 3 different ADCs to digitize the three axes of the gyroscope.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
May 26, 2025

Hi @fgs ,

The LPF2 is not configurable and the cutoff frequency depends on the ODR_G.

There are 3 different ADCs to digitize the three axes of the gyroscope.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
fgsAuthor
Associate II
May 26, 2025

Thank you !