Associate II
October 19, 2022
Question
lsm6dsl AWT interrupt
- October 19, 2022
- 0 replies
- 811 views
hello
i use STEVAL-MKI178V2 (adapter board) + STEVAL-MKI109V3 (motherboard) with UNICO-GUI ver9.13.
i try "Absolute wrist tilt" example as it described in "AN5040 - Rev 3".
The questions are:
- in "A_WRIST_TILT_Mask (59h)" register, each bit by itself works fine. but if i use more than 1 axis (x and y, or y and z) - i got continuous interrupts (interrupt than latency time than interrupt ...). see attached picture
- in "A_WRIST_TILT_Mask (59h)" register, for each axis i got absolutely same behavior for positive and negative tilt.
please advice
Alexander