LSM6DSL Interrupt Generation -- Interrupts constantly fire
I'm trying to get the Activity/Inactivity interrupt generation on the LSM6DSL working. I've implemented the example code in the data sheet below. I'm using an stm32L475.
However, this interrupt fires constantly, regardless of either the sleep duration time or the activity threshold. From reading the SLEEP_STATE_IA from the WAKE_UP_SRC register, it also appears to always be the inactivity interrupt firing, not the activity one.
In trying to debug this, I also tried implementing the other interrupt generators (Free Fall, Single Tap, etc...). These interrupts also constantly fired, regardless of their configurations.
However, when I tried implementing the Data Ready Interrupt, it worked correctly. I even slowed the accelerometer down to 1.6Hz to verify.
So what am I doing wrong for interrupt generation? Is my GPIO interrupt line maybe messed up?
Example Free Fall code:
uint8_t data1[2] = {CTRL1_XL, 0x50};
i2c_transaction(WRITE_ADR, WRITE_I2C, data1, 2);
// 2. Write 02h to WAKE_UP_DUR
uint8_t data2[2] = {WAKE_UP_DUR, 0x02};
i2c_transaction(WRITE_ADR, WRITE_I2C, data2, 2);
// 3. Write 02h to WAKE_UP_THS
uint8_t data3[2] = {WAKE_UP_THS, 0x02};
i2c_transaction(WRITE_ADR, WRITE_I2C, data3, 2);
// 4. Write E0h to TAP_CFG
uint8_t data4[2] = {TAP_CFG, 0xE0};
i2c_transaction(WRITE_ADR, WRITE_I2C, data4, 2);
// 5. Write 80h to MD1_CFG
uint8_t data5[2] = {MD1_CFG, 0x80};
i2c_transaction(WRITE_ADR, WRITE_I2C, data5, 2);
------------------------------------------------------------------------
My interrupt line config:
// GPIO D11 is the I2C interrupt line for LSD6DSL
RCC->AHB2ENR |= RCC_AHB2ENR_GPIODEN;
RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;
// Clear mode bits (and also set to input mode 00)
GPIOD->MODER &= ~(GPIO_MODER_MODE11_Msk);
GPIOD->PUPDR &= ~(GPIO_PUPDR_PUPD11_Msk);
GPIOD->PUPDR |= (GPIO_PUPDR_PUPD11_1);
SYSCFG->EXTICR[2] |= SYSCFG_EXTICR3_EXTI11_PD;
EXTI->IMR1 |= EXTI_IMR1_IM11;
EXTI->RTSR1 |= EXTI_RTSR1_RT11;
NVIC_EnableIRQ(EXTI15_10_IRQn);
NVIC_SetPriority(EXTI15_10_IRQn, 0); // Adjust priority as needed
------------------------------------------------------------------------------------------
My interrupt handler:
void EXTI15_10_IRQHandler(void) {
if (EXTI->PR1 & EXTI_PR1_PIF11) { // Check if PD11 triggered the interrupt
read_xl = 1;
EXTI->PR1 = EXTI_PR1_PIF11;
}
}
Thanks!